| Subject | Author | Posted | |
|---|---|---|---|
|
Greetings, I am working on a Firmware OTA module for STM32L4 series and for that I need a module t...
| 2024-03-27 11:47 PM | ||
|
This is an example of what I try to do with the DFSDM without success. I want to apply a low pass ...
| 2024-03-27 4:00 PM | ||
|
Hello dear community, I’m working on a USB sound interface, using a STM32F7 and an external DAC ch...
| 2024-03-27 8:26 AM | ||
|
I have a use case for communicating with the SDRAM chip onboard the STM32G474E-EVAL1 board. Took a...
| 2024-03-27 7:14 AM | ||
|
Edit: I found the problem, and it is of course my own fault. Careful reading of the transceiver chi...
| 2024-03-26 7:25 AM | ||
|
hi, how to clean SRAM before jumping to main application from bootloader . In the SD card boot lo...
| 2024-03-26 4:23 AM | ||
|
Hi, Currently I am working with STM32L4R9 Discovery kit. The connected PSRAM model with this board...
| 2024-03-25 5:55 PM | ||
|
I finished my I2C peripheral drivers and I would like to test it with my bh1750 sensor but I am hav...
| 2024-03-25 5:51 PM | ||
|
stm32l071CB flash only 128kB, can fatfs run on Stm32L071CB? Roughly how much space it takes up?The ...
| 2024-03-24 6:18 PM | ||
|
Hi All I am working on a data logger code. It is basic at the moment. 1, set a an ISRTimmer for 1...
| 2024-03-23 5:58 PM | ||
|
Hi all. We are using a bidirectional UART with hardware-flow control lines (RTS/CTS) between two m...
| 2024-03-21 4:25 AM | ||
|
Hello, I have 10 devices STM32L496VG in Dual-Bank-Boot mode with the identical firmware in BANK1 a...
| 2024-03-20 4:21 PM | ||
|
DSI2HDMI display converter - SL-MIPI-LVDS-HDMI-CNV (somlabs.com) how can i interface lvds displa...
| 2024-03-19 6:02 AM | ||
|
Hello! I would like to test it using STEVAL-FKI915V1(S2-LP). -. Setting conditions: 1) Frequency...
| 2024-03-18 11:59 PM | ||
|
Hello, I use STM32F429IGT6 MCU I am trying to communicate with TI's DLPC through HW connection. ...
| 2024-03-17 11:32 PM | ||
|
hi, that's the first time a i wrote to this comunity because i'm stuck with this *** problem since ...
| 2024-03-17 2:41 AM | ||
|
Dear expert I am currently implementing the SMBUS communication with TI BQ40Z80 via STM32L431xxx +...
| 2024-03-15 12:55 AM | ||
|
Hello STM32 Community, I am currently working on a project where I’m trying to test I2S communicat...
| 2024-03-14 5:15 AM | ||
|
Hello I am trying to do spi_dma communication using the HAL_SPI_TransmitReceive_DMA function. ...
| 2024-03-14 1:59 AM | ||
|
Hi all, I used long time STM32F103 and there was the possibilty to release the CAN Fifo by writing...
| 2024-03-14 12:41 AM |