| Subject | Author | Posted | |
|---|---|---|---|
|
Hello, I use STM32F429IGT6 MCU I am trying to communicate with TI's DLPC through HW connection. ...
| 2024-03-17 11:32 PM | ||
|
hi, that's the first time a i wrote to this comunity because i'm stuck with this *** problem since ...
| 2024-03-17 2:41 AM | ||
|
Hello! We are trying to implement a project that involves the STM32F429 microcontroller and the pro...
| 2024-03-15 2:50 AM | ||
|
Dear expert I am currently implementing the SMBUS communication with TI BQ40Z80 via STM32L431xxx +...
| 2024-03-15 12:55 AM | ||
|
Hello STM32 Community, I am currently working on a project where I’m trying to test I2S communicat...
| 2024-03-14 5:15 AM | ||
|
Hello I am trying to do spi_dma communication using the HAL_SPI_TransmitReceive_DMA function. ...
| 2024-03-14 1:59 AM | ||
|
Hi all, I used long time STM32F103 and there was the possibilty to release the CAN Fifo by writing...
| 2024-03-14 12:41 AM | ||
|
Hi, I need help on MMC operations. My project is using STM32U575 to access MMC chip (EMMC16G-IB29...
| 2024-03-13 5:25 AM | ||
|
Hi, I have configured the Nucleo-L476RG to write to a 64GB exFat Micro SD Card in 4-bit mode using...
| 2024-03-12 6:50 AM | ||
|
I was able to create a cmake template project. but in this project i didn't find the .ioc file and ...
| 2024-03-11 4:44 PM | ||
|
Has anyone ever had success getting the CS42L52 audio CODEC to work on the MCBSTM32F400 board? It i...
| 2024-03-11 7:39 AM | ||
|
I am trying to use tickless idle mode. But for some reason I cant go into sleepmode, the mcu instan...
| 2024-03-11 5:55 AM | ||
|
I want to make a structured project for stm32 with cmake where I want to make A parent folder like ...
| 2024-03-09 9:46 AM | ||
|
Hello everyone, I just started using stm32cubeide. I'm trying to do I2S protocol. I'm trying to f...
| 2024-03-08 3:22 AM | ||
|
Hello, I have created a bootloader application that jumps to main application at 0x08010000. It w...
| 2024-03-06 3:54 AM | ||
|
I have developed a custom controller that uses the STM32G474RE to regulate the output voltage of tw...
| 2024-02-29 3:12 AM | ||
|
I'm seeing strange behavior trying to write to the ADC1_JSQR register. This register controls the c...
| 2024-02-27 2:27 PM | ||
|
hello
i wand to use stm32h7 series LQFP package to connect RGB888 display
first time i try with...
| 2024-02-27 12:10 AM | ||
|
I need live time from ntp server and we trying to read to read the response after sending a 48 char...
| 2024-02-26 1:13 AM | ||
|
You don't initialize sFilterConfig to zero, so sFilterConfig.FilterMaskIdLow could be a random numb...
| 2024-02-16 5:26 PM |