| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, now I'm implementing i2c with 1 master(U575ZI-Q) and 3 slave(L432KC) boards. master transm...
| 2024-05-07 6:40 PM | ||
|
Hi, I am using the STM32H750B-DK board and would like to use the LCD and touch screen in my pro...
| 2024-05-07 10:43 AM | ||
|
hi, i use sbsfu bootloader, the problem was the boot don't found the image. i used Ymodem to send...
| 2024-05-07 9:09 AM | ||
|
Hey all, Would I be able to use a Bluetooth module to view video stream from camera module in orde...
| 2024-05-06 11:43 AM | ||
|
Hi everyone, i am using stm32g0c1retx MCU for i2c communication in slave mode. in normal mode i am...
| 2024-05-06 5:27 AM | ||
|
Hello, maybe a lame question, but how to force enable SWV even if the microcontroller in the projec...
| 2024-05-06 3:07 AM | ||
|
Hello, I'm implementing the management of an SD Card using a micro STM32H7xx. While analyzing the ...
| 2024-05-03 7:35 AM | ||
|
Hi everybody, I have a lot of the same warnings, but the compilation is ok! I would still like to ...
| 2024-05-03 1:53 AM | ||
|
Hi. I am working with STM32G473 for a safety application. I cant find a reference to how the so...
| 2024-05-02 10:37 AM | ||
|
Greeetings, I'am currently working on a project consisting on acquiring a TTL signal which coul...
| 2024-05-01 10:59 AM | ||
|
Hi, when investigating issues with the DMA, i found, that the prescaler is not working properly. ...
| 2024-05-01 10:46 AM | ||
|
Hi,
The propagation delay and offset error mentioned below for integgrated comparator.
Can it b...
| 2024-04-30 12:53 AM | ||
|
I'm working with stm32f0 hdmi cec function to make Arc audio with tv I can able to communicate wit...
| 2024-04-28 12:39 AM | ||
|
I have a custom board using the STM32L562Q BGA package processor. I have a high speed capable eMMC...
| 2024-04-27 9:23 AM | ||
|
I am configuring STM32L496ZGP as an I2C Slave. Master is a software(i.e.)Aardvark Total Phase Contr...
| 2024-04-27 4:25 AM | ||
|
I've been testing the ADC_RESOLUTION_14B_OPT mode of the H743VIT6 ADCs but I cannot see any changes...
| 2024-04-27 4:07 AM | ||
|
Hi all, I tried to configure the clock to run at 32MHz and I was using Systick to toggle the LED ev...
| 2024-04-27 12:19 AM | ||
|
Hi, I am trying to interface FM18W08 FRAM from Cypress using FMSC in the STM32F303ZE board. I feel...
| 2024-04-26 11:02 PM | ||
|
Hello everyone, I am new to the world of STM32 and am trying to get a bit familiar with the topic. ...
| 2024-04-26 1:58 PM | ||
|
Hello, Am using STM32H7 and STM32G4 devices and need bluetooth connectivity and USB storage driver...
| 2024-04-24 9:47 PM |