Dear all, on a custom board based on STM32MP157D I successfully managed to configure an LCD display that works perfectly using "modetest -s" and "psplash-drm". But I cannot run the examples in the s...
0 Hi I am trying to write a c/c++ application which will excercise the Tx and Rx pins of the can interfaces (can0 and can1) available in the STM32MP157CAA. Approach One I wrote an applicat...
Hello, I am developing on a custom STM32MP151AAC board, the software is openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23. The board successfully booted, and most of the part works fine. The probl...
Hello Madam/sir,
Recently we have purchased STM32MP157F-DK2 development board, and we are very new to this board. We are trying to install PyQt5 on this board but we are getting error "Package not ...
Hello. I'm currently trying to download the X-LINUX-AI package for MPU ecosystem v5.0.0. I tried on MP135F-DK & MP157F-DK2, but neither showed a valid installation and both were stuck when exec...
I've been trying to cross compile pyzmq for my stm32mp135f-dk and I'm facing issues with it. I've ran the script to setup my environment for the SDK. And made the required changes in the setup...
Hello, I was wondering by using X-AI package. Will I be able to use the XGboost model converted to ONXX format in STM32 MP157 A7 core. Or it only supports Neural Network models?  ...
Hi, we are currently porting a custom dunfell distro from STM32MP151A to STM32MP151C. We followed the guides related to creating our own machine by generating the device tree in CubeMX and succeede...
Hi! I have tried to compile OP-TEE version 3.19.0-stm32mp-r1.1 for the STM32MP157F-DK2 board. With the official source on STMicroelectronics OP-TEE Github repo ,but I get the ...
Hi all! Environment: I use MX to configure the DCMI Peripheral including DMA! MX generates MX_DMA_Init() and MX_DCMI_Init() After DCMI initialization in main with the above mentioned functions I...