Hi all, I'm trying add FPU exception to my project and I'm bit confused because two sources points two different interrupt vectors for this. Book E says, FPU exception is under IVOR33 but SPC58xH ma...
Hi, I have been working with the board for quite some time and everything was functioning normally. Last day, upon powering the board, I noticed that the board has entered reset mode. Also, I have be...
Hi I need to flash via CAN bus and I understood it is possible using SPC5-FLASHER on PC connected to the target via USB/CAN interface with SPC5_UPDATER_CONN=SPC5_UPDATER_CONN_CAN. &nbs...
I want to flash and debug using SPC5-UDESTK 5.02.04 on to the board SPC5746CBMKU6. This controller configuration is not given in the tool. So I have created new configuration for this ...
Hi I'm working with SPC570 and SPC5 Studio, version: 5.8.1 with installed the SPC5Studio patch for DMA in SPC570S DSPI lld running on Windows 11. Very often I have a problem with ...
Hello there i have maserati levante modena 2022 SUV and it’s totally flooded.BCM also totally damaged.BCM mcu is ST spc5605bmlu6.I couldn’t find any application to read and re-write this mcu.does an...
Hi, I'm using TMS570 with SPC5STUDIO environment. My toolchain generates out.elf and out.hex but I would like to have a byte hex stream (without address and other information) directly do us...
Hi guys, I'm using RM0421 as reference for my develop work. But find some error in Chapter 5.1 Table 6. The end address of 256KB Code Flash block 4 and block 5 should be 0x0113FFFF and 0x0...