Resolved! How to install pip or python package (as pyserial.py)
Hi,How can I install pyserial.py python modul on Discovery kit STM32MP135F.I would like also install pip Thank you for your help.Olivier
Hi,How can I install pyserial.py python modul on Discovery kit STM32MP135F.I would like also install pip Thank you for your help.Olivier
Hi everyone,we are in the middle of bringing up a custom board using the STM32MP131. Booting from an SD card already works. However, we would like to use the STM32CubeProgrammer to directly connect the board via USB. For this, the OTG USB pins OTG_HS...
Greetings. We are currently working on a project related to the board STM32MP135F-DK. We are seeking your assistance to clarify a few points. Specifically, we would like to know which primary images are necessary for this board and which operating sy...
Hello, I am working on STM32MP135-dk board.i am running make command but its not working, it shows fatal error: XDisplayInfoHeader.h: No such file or directory, this error. How to solve it ? i am sharing some screenshots below.
I have a simple recipes, which used to install certain files to rootfs, as below:DESCRIPTION = "A hello world example"SECTION = "appauto"DEPENDS = ""LICENSE = "CLOSED"FILESEXTRAPATHS:append := ":${THISDIR}/file"SRC_URI = "file://hello.service \"do_in...
i am using stm32mp135-dk board. i have installed STM32MP1-Ecosystem-v5.0.0 Starter Package now i want to create GUI with guizero what i do ?
Hi Team, I am working on DDR3L batch simulation in Hyperlynx with STM32MP131 series processor. While assigning the appropriate ODT models, I am getting some errors with respect to IBIS model. So please help me in rectifying the issuesPFA error log as...
i am using stm32mp135-dk board . i have installed the STM32MP1-Ecosystem-v5.0.0 Starter Package now i want to install python how i can install ?
i am using stm32mp135-dk board i am install the STM32MP1-Ecosystem-v5.0.0 Starter Package now i want to connect the board with my laptop using putty software ,i have the ip address of the board but did't have the password of the board. what will ...
i have download the embedded wizard example from https://www.embedded-wizard.de/platforms/stmicroelectronics/stm32mp1 this website.now i am confusing that how i can run this builed example in stm32MP135 ?