2024-06-04 09:03 AM
Example image without zoom controll
Re: ThreadX thread and queue names not displayed p... - STMicroelectronics Community
example with zoom controll i cant found now , but sometimes is showed bottom on image
and i mean this zoom control is required on all any image.
2024-06-07 02:45 AM
Hello @MM..1 ,
Thanks for sharing your request. I will see what we can do about it and get back.
In the meantime, I suggest using a workaround following these steps:
1. Right mouse click on the image
2. Select "Magnify image"
This will allow you to have a zoom in / zoom out option.
Cheers,
Lina
2024-06-07 06:17 AM
Definitely see inconsistency, perhaps related to the image type. ie for PNG but not JPG ?
Also find the two-point finger stretching on Android is frustrating, and also having to down load attached images to see them.
2024-07-23 09:33 AM
Hi @MM..1 @Tesla DeLorean ,
Could you please share a direct link when you come across an image with the zoom control you are referring to? We need an example to be able to investigate it.
Best,
Adam
2024-07-23 10:04 AM
Error in final launch sequence - STMicroelectronics Community attached png show zoom
normal images no. But on my notebook with 2560x1440 14inch is ...
2024-08-13 01:24 AM
Hi @MM..1 ,
Zoom controller is currently only available for file attachment previews. We will pass along the topic to the developer team to understand the effort involved in adding a zoom controller for images in posts. Depending on the estimation, we will decide how to move forward with this topic. We will keep you posted.
Best,
Adam