2024-06-04 09:03 AM
Example image without zoom controll
Re: ThreadX thread and queue names not displayed p... - STMicroelectronics Community
example with zoom controll i cant found now , but sometimes is showed bottom on image
and i mean this zoom control is required on all any image.
2024-06-07 02:45 AM
Hello @MM..1 ,
Thanks for sharing your request. I will see what we can do about it and get back.
In the meantime, I suggest using a workaround following these steps:
1. Right mouse click on the image
2. Select "Magnify image"
This will allow you to have a zoom in / zoom out option.
Cheers,
Lina
2024-06-07 06:17 AM
Definitely see inconsistency, perhaps related to the image type. ie for PNG but not JPG ?
Also find the two-point finger stretching on Android is frustrating, and also having to down load attached images to see them.