cancel
Showing results for 
Search instead for 
Did you mean: 

What is the timezone of this forum?

Uwe Bonnes
Principal III

What is the time zone of the forum. My last complaint is tagged "2024-05-01 5:21:40 AM" while here it is about 12:23:34 UTC 2024.

 

Please tag the posting explicit with the tinmezone!

15 REPLIES 15
Andrew Neil
Evangelist III

I have never understood what timezone the forum is using!

It's certainly no timezone anywhere near the one I'm actually in (UK)!

 

EDIT:

It's tagged this as 06:06 AM - it's actually 14:06 BST here.

Andrew Neil
Evangelist III

Also, if you're going to present times as, eg, "06:06" then the leading zero indicates that it's 24 hours - so the AM should not be there.

"06:06 PM" should never be seen! 

Ok, im not far away , Germany . Here summertime (+1h) , now 15:31 .

ed

forum shows 03:31 PM.

so we know... :)

ed2

AScha3_0-1714570402774.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Looks to be Pacific Time / California (GMT-8)

08:33 in Chicago, 06:33 in San Jose

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Can be changed via My Settings -> Preferences -> Time Zone

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Right. So it shows - what time zone is set in My Settings -> Preferences -> Time Zone .

If you feel a post has answered your question, please click "Accept as Solution".

Under 'Personal' I had my location set as GB - but it doesn't base the default timezone on that, of course.

:face_with_rolling_eyes:

Changed Time Zone under 'Preferences'  to "GMT" - will that adjust for BST ... ?

:thinking_face:

 

edit:

Yes, it is now showing BST. :thumbs_up:

But saying "03:08 PM". :thumbs_down:

Uwe Bonnes
Principal III

Any opinions on this subject from STM side?

Will be system default when not logged in.

 

@Lina_DABASINSKAITE @STTwo-32 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..