2024-05-01 5:25 AM - edited 2024-05-01 5:26 AM
What is the time zone of the forum. My last complaint is tagged "2024-05-01 5:21:40 AM" while here it is about 12:23:34 UTC 2024.
Please tag the posting explicit with the tinmezone!
2024-05-01 6:06 AM - edited 2024-05-01 6:07 AM
I have never understood what timezone the forum is using!
It's certainly no timezone anywhere near the one I'm actually in (UK)!
EDIT:
It's tagged this as 06:06 AM - it's actually 14:06 BST here.
2024-05-01 6:15 AM
Also, if you're going to present times as, eg, "06:06" then the leading zero indicates that it's 24 hours - so the AM should not be there.
"06:06 PM" should never be seen!
2024-05-01 6:31 AM - edited 2024-05-01 6:33 AM
Ok, im not far away , Germany . Here summertime (+1h) , now 15:31 .
ed
forum shows 03:31 PM.
so we know... :)
ed2
2024-05-01 6:33 AM - edited 2024-05-01 6:34 AM
Looks to be Pacific Time / California (GMT-8)
08:33 in Chicago, 06:33 in San Jose
2024-05-01 6:38 AM
Can be changed via My Settings -> Preferences -> Time Zone
2024-05-01 6:44 AM
Right. So it shows - what time zone is set in My Settings -> Preferences -> Time Zone .
2024-05-01 7:08 AM - edited 2024-05-01 7:12 AM
Under 'Personal' I had my location set as GB - but it doesn't base the default timezone on that, of course.
:face_with_rolling_eyes:
Changed Time Zone under 'Preferences' to "GMT" - will that adjust for BST ... ?
:thinking_face:
edit:
Yes, it is now showing BST. :thumbs_up:
But saying "03:08 PM". :thumbs_down:
2024-05-14 9:04 AM
Any opinions on this subject from STM side?
2024-05-14 9:29 AM
Will be system default when not logged in.