2023-11-30 02:55 PM - edited 2023-12-01 08:47 AM
https://community.st.com/t5/badges/userbadgespage/user-id/33216/page/1
Basically Gamification Failure, nothing above 50/100 levels
2023-12-13 06:07 AM
Thanks, @Tesla DeLorean , for this cute reference. More badgers to come in 2024 :grinning_face_with_sweat:
2023-12-13 06:28 AM - edited 2023-12-13 06:28 AM
they should name a badge after you
2023-12-13 07:58 AM
I think one of the other posters kept referring to them as "badgers" and I think it works well as a meme..
To be honest I think this gamification is a bit pointless, but I just feel that I've reached to the end of the internet here..
2023-12-13 07:59 AM
https://fantasticmrfox.fandom.com/wiki/Clive_Badger
2023-12-13 08:19 AM - edited 2023-12-13 08:20 AM
>>I've reached to the end of the internet here..
you kind of have, time to start to reply to posts in with criptic meta-memes.
>>gamification is a bit pointless
i feel this is just a marketing stunt with no real value , like commertials in the 90s selling car insurance with rap music.
Completely missunderstanding their public
2024-01-10 05:48 AM
Thanks for the link.
2024-01-19 03:13 AM
@Javier1 wrote:Completely missunderstanding their public
Indeed - do they think we're 10-year-old boy scouts from the 70s keen to collect all these "badges"?
2024-03-07 08:53 AM
Tis still brocken..
2024-04-17 09:25 AM
Approaching 2000 solutions. Khoros NIL
When it comes to forum software vendors how do we keep picking complete donkeys?