cancel
Showing results for 
Search instead for 
Did you mean: 

multiple notifications for the same post

Andrew Neil
Evangelist III

These two notifications refer to the exact same post:

AndrewNeil_0-1707917580502.png

He couldn't have mentioned me without making a reply, so I really don't need two separate notifications!

EDIT

And why are the two email notifications sent 7 minutes apart?!

AndrewNeil_0-1707917914560.png

 

2 REPLIES 2
Laurids_PETERSEN
Community manager
Community manager

Hi @Andrew Neil,

Thanks for your feedback. 

Given that the notifications are triggered separately there is no immediate fix/workaround to this issue. 

We can look into scenarios where only one notification is necessary in general. I can't promise we can change anything soon, but the feedback is noted. 

Best regards,
Laurids 
 


@Laurids_PETERSEN wrote:

the notifications are triggered separately the


Why?

Here we see that notifications can be combined:

https://community.st.com/t5/feedback-forum/notification-feed-corrupted/m-p/703905/highlight/true#M1597

@Lina_DABASINSKAITE