2026-03-12 4:14 AM
I get this error when I press the 'Kudos' button:
Also happens on other posts in that thread, and in other threads.
Looks like a recurrence of Kudos button gives error (12 Dec 2025)
Solved! Go to Solution.
2026-04-21 2:56 AM
Hi @Andrew Neil,
The troubleshooting team got back confirming issue was caused due to the server error that day which is now fixed. The feature should work as expected.
Let me know if it works well on your side.
Thanks,
Lina
2026-03-12 7:16 AM
I've experienced this in the morning (at a different post), but it appears to have healed itself since then :)
JW
2026-03-12 7:23 AM
I just managed to Kudo your post.
So I checked others - they are also working now.
2026-03-12 7:57 AM
I spoke too soon - I am unable to kudo *your* above post!
Please un-mark my post (even if it's hard to find :) ).
JW
2026-03-12 8:04 AM
I could Kudo your latest post, but have unmarked the solution anyhow - for now ...
2026-03-12 8:17 AM
Hi @Andrew Neil,
Thanks for reporting this. I'm sorry about the inconvenience.
I faced the same issue with that specific reply. I have captured the needed log files for support to investigate further.
I'll report back once I have any news.
2026-03-12 10:12 PM
Kudos seems working for me now.
2026-03-13 2:58 AM - edited 2026-03-13 3:00 AM
Kudos button failed for me just now
Post: https://community.st.com/t5/stm32cubeide-mcus/stm32-cubeide-how-to-modify-c-language-parallel-compilation/m-p/885583/highlight/true#M41330
2026-03-13 4:24 AM
And now it's stopped working again for me.
Including trying to UN-Kudo @unsigned_char_array's post above (not any reflection on the content - purely as a test of the Kudo functionality!)
2026-03-13 6:17 AM
It works again for me.