cancel
Showing results for 
Search instead for 
Did you mean: 

Validation error on target

RGura.1096
Associate II

I need help. I am trying to validate on target : STM32L476RG nucleo board.

E200(ValidationError): stm32: Unable to bind the STM AI runtime with "network" c-model: [] 

 connection to "serial:COM4:115200"/"COM4:115200" run-time fails 

 E801(HwIOError): Invalid firmware - COM4:115200 

No model runs.

3 REPLIES 3
Imen.D
ST Employee

Hello @RGura.1096​ ,

Which version of AI package and tool are you using ?

Please, make sure to use the latest version, if it's not done.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Snara.21
Senior

@Imen DAHMEN​  I am also facing the same issue. Kindly help it is the latest version

aben118
Associate II

what is the solution to this please? i am also using the latest version