2024-01-11 06:18 AM
Hi all,
I installed Unicleo-GUI on my Windows laptop, and was able to read sensor data from my NUCLEO-IKS01A3 board successfully. The board was automatically identified by the software as being connected to COM4 yesterday. For some reason today the software recognizes the COM connection but not the board and thus won't display the data being read by it on the screen.
I have tried reinstalling Unicleo as well as the FP-SNS-DATALOG2 function pack with no success.
Any advice or suggestions are appreciated!!
Solved! Go to Solution.
2024-01-11 06:54 AM
The firmware from FS-SNS-DATALOG2 is not compatible with Unicleo-GUI. Compatible firmware is in X-CUBE-MEMS1 package.
2024-01-11 06:54 AM
The firmware from FS-SNS-DATALOG2 is not compatible with Unicleo-GUI. Compatible firmware is in X-CUBE-MEMS1 package.
2024-02-01 01:08 AM
Hi @ZoeTakacs ,
Did you try to use the compatible firmware that Miroslav suggested you?
If yes, remember to click the 'accept as solution' button on his answer to be of help to other users :)