Undefined reference from AI model generation with X-CUBE-AI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-04 1:03 AM
Hi,
I am following this tutorial to use my own image recognition model with the STM32H747I-DISCO board. I have already ran the demos and they seem to work fine.
I first configure the model in CUBE-MX successfully and then copy the required files to the demo project.
When I compile the code in the STM-IDE I get the following error a bunch of times:
undefined reference to `forward_conv2d_if32of32wf32'
I also get this:
STM32H747I_DISCO_PersonDetect_Google_CM7.elf section `.bss' will not fit in region `DTCMRAM'
STM32H747I_DISCO_PersonDetect_Google_CM7.elf section `.axiram_section' will not fit in region `AXIRAM'
STM32H747I_DISCO_PersonDetect_Google_CM7.elf section `.sram_section' will not fit in region `SRAM123'
section .axiram_section VMA [24000000,241ad7ff] overlaps section .bss VMA [20017a40,2c6301a7]
even though CUBE-MX said that the used memory is within the flash and ram available (as shown in the image included).
The declaration is in layers_conv2d.h but I can't find the definition anywhere.
I have done the Updating to a newer version of X-CUBE-AI part in the tutorial successfully.
Any ideas?
thanks
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-07 7:32 AM
Hello @dogg ,
I don't know about a lower limit concerning data, I will ask the dev team.
Concerning the quantization, if everything went correctly, you should have a .tflite model in /experiment_output/<date of experiment>/quantized_model.
You can try to use only the quantization operation mode:
- Add a quantization path in the dataset part of the yaml, it is advised to put the training data.
- You may need to use the model_path in the general part and comment everything from training/model:
general:
project_name: COCO_2017_person_Demo
model_type: st_ssd_mobilenet_v1
model_path: <PATH TO YOUR TRAINED MODEL>
logs_dir: logs
saved_models_dir: saved_models
gpu_memory_limit: 12
global_seed: 127
operation_mode: quantization
training:
# model:
# type: st_ssd_mobilenet_v1
# alpha: 0.25
# input_shape: (256, 256, 3)
# weights: None
# pretrained_weights: imagenet
...
Leave everything else the same.
If it doesn't work, you can also try to use the ST Edge AI Dev cloud to do the quantization instead of the local installation of ST Edge AI. Just change on_cloud to True. (you need a st accound and you will be ask to log after running the python script)
tools:
stedgeai:
version: 9.1.0
optimization: balanced
on_cloud: True
path_to_stedgeai: C:/Users/haris/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/9.1.0/Utilities/windows/stedgeai.exe
path_to_cubeIDE: C:/ST/STM32CubeIDE_1.16.1/STM32CubeIDE/stm32cubeide.exe
Finally, if it does not work, you can also quantize it manually on the ST Edge AI Dev Cloud
Documentation: https://wiki.st.com/stm32mcu/wiki/AI:Getting_started_with_STM32Cube.AI_Developer_Cloud
Let me know if it helps.
Julian
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 6:40 AM
Hello @dogg ,
We are working on this tutorial to replace it with model zoo.
I don't know if you are familiar with model zoo but to replicate the tutorial you are following, in your place I would:
- Follow the train readme to retrain a model with your data: stm32ai-modelzoo/object_detection/src/training/README.md at main · STMicroelectronics/stm32ai-modelzoo · GitHub
- Follow the deploy readme to deploy it on your board:stm32ai-modelzoo/object_detection/deployment at main · STMicroelectronics/stm32ai-modelzoo · GitHub
You can have a look on a similar thread where I describe how to replicate the object detection function pack:
Solved: stm32ai-modelzoo flash pre-trained model example. - STMicroelectronics Community
- Here I explain how to install "st edge ai" for local quantization
- Explain how to get a pretrained model from model zoo
- deploy it
It is quite similar to your issue I believe.
Have a good day,
Julian
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 6:46 AM
Hello dogg,
The situation triggers me an idea.
Between the versions of X-CUBE-AI, the implementation of the AI kernels is continuously improving.
Your problem sounds like a misalignment between C, H, and lib files of X-CUBE-AI versions that you have inside your project. May be you have, during your exploration, ended to a situation where one file is from a different version.
I would erase all the X-CUBE-AI files from your project and redo the integration.
I hope it will help
With Kind Regards,
Nicolas_V
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 7:07 AM
Hi,
Thanks for the support, I have already deleted and recreated it a few times but will try a fresh try once more.
Are you saying that the same can be done with the model zoo? Transferring my own model to the development board?
I will investigate on that too and get back to you here.
thanks again
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-06 6:16 AM - edited ‎2024-11-07 1:21 AM
Hi again,
I have managed to make the deployment example work on my disco board and have also managed to train sd_ssd_mobilenet_v1 on the pascal dataset. The output is a .h5 file however and I haven't managed to get a .tflite version. Can that be done automatically? I am having trouble with a generic converter python script getting this error:
Exception encountered: Unrecognized keyword arguments passed to DepthwiseConv2D: {'groups': 1}
I also tried training that model on my own dataset with yolo annotations but I get this error:
FileNotFoundError: [Errno 2] Unable to synchronously open file (unable to open file: name = 'C:\Users\Haris\Desktop\stm32ai-modelzoo\object_detection\src\experiments_outputs\2024_11_06_16_14_16\saved_models\best_weights.h5', errno = 2, error message = 'No such file or directory', flags = 0, o_flags = 0)
this is my yaml file for training from scratch:
general:
project_name: COCO_2017_person_Demo
model_type: st_ssd_mobilenet_v1
# model_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/pretrained_models/st_ssd_mobilenet_v1/ST_pretrainedmodel_public_dataset/coco_2017_person/st_ssd_mobilenet_v1_025_256/st_ssd_mobilenet_v1_025_256.h5
logs_dir: logs
saved_models_dir: saved_models
gpu_memory_limit: 12
global_seed: 127
operation_mode: training
#choices=['training' , 'evaluation', 'deployment', 'quantization', 'benchmarking',
# 'chain_tqeb','chain_tqe','chain_eqe','chain_qb','chain_eqeb','chain_qd ']
# dataset:
# name: COCO_2017_person
# class_names: [ person ]
# training_path:
# validation_path:
# test_path:
# quantization_path:
# quantization_split: 0.3
dataset:
name: bugs # Dataset name. Optional, defaults to "<unnamed>".
class_names: [nc, mr, wf] #[ aeroplane,bicycle,bird,boat,bottle,bus,car,cat,chair,cow,diningtable,dog,horse,motorbike,person,pottedplant,sheep,sofa,train,tvmonitor ] # Names of the classes in the dataset.
training_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/src/bugs/train
validation_path: C:/Users/Haris/Desktop/stm32ai-modelzoo/object_detection/src/bugs/valid
validation_split: 0.2 # Training/validation sets split ratio.
test_path:
quantization_path:
quantization_split: # Quantization split ratio.
seed: 123 # Random generator seed used when splitting a dataset.
preprocessing:
rescaling: { scale: 1/127.5, offset: -1 }
resizing:
aspect_ratio: fit
interpolation: nearest
color_mode: rgb
data_augmentation:
rotation: 30
shearing: 15
translation: 0.1
vertical_flip: 0.5
horizontal_flip: 0.2
gaussian_blur: 3.0
linear_contrast: [ 0.75, 1.5 ]
training:
model:
type: st_ssd_mobilenet_v1
alpha: 0.25
input_shape: (256, 256, 3)
weights: None
# pretrained_weights: imagenet
dropout:
batch_size: 12
epochs: 1
optimizer:
Adam:
learning_rate: 0.001
callbacks:
ReduceLROnPlateau:
monitor: val_loss
patience: 20
EarlyStopping:
monitor: val_loss
patience: 40
postprocessing:
confidence_thresh: 0.6
NMS_thresh: 0.5
IoU_eval_thresh: 0.3
plot_metrics: True # Plot precision versus recall curves. Default is False.
max_detection_boxes: 10
quantization:
quantizer: TFlite_converter
quantization_type: PTQ
quantization_input_type: uint8
quantization_output_type: float
granularity: per_channel #per_tensor
optimize: False #can be True if per_tensor
export_dir: quantized_models
benchmarking:
board: STM32H747I-DISCO
tools:
stedgeai:
version: 9.1.0
optimization: balanced
on_cloud: False
path_to_stedgeai: C:/Users/haris/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/9.1.0/Utilities/windows/stedgeai.exe
path_to_cubeIDE: C:/ST/STM32CubeIDE_1.16.1/STM32CubeIDE/stm32cubeide.exe
deployment:
c_project_path: ../../stm32ai_application_code/object_detection/
IDE: GCC
verbosity: 1
hardware_setup:
serie: STM32H7
board: STM32H747I-DISCO
mlflow:
uri: ./experiments_outputs/mlruns
hydra:
run:
dir: ./experiments_outputs/${now:%Y_%m_%d_%H_%M_%S}
thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-07 5:25 AM
Hello @dogg ,
There are different operation mode, you used training that just retrain a model, here are all the operation modes:
https://github.com/STMicroelectronics/stm32ai-modelzoo/tree/main/image_classification
What I generally do is chain_tbqeb to do everything in one go: to train, benchmark the memory, inference time etc, quantize, evaluate the performance and do a new benchmark to see the difference between the .h5 and the .tfile.
You can use the quantize in your case.
For your first error, I am not sure what caused this, I never used the scripts other than the stm32ai_main.py
For the second error, it seems that a path is wrong and the file cannot be found.
The deployment operation mode generate a binary file flashed directly. If you want to generate a cubeIDE project or cubeMX project, you can take a look at the ST Edge AI Dev Cloud
https://wiki.st.com/stm32mcu/wiki/AI:Getting_started_with_STM32Cube.AI_Developer_Cloud
Have a good day,
Julian
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-07 7:07 AM
Hello,
I've managed to train the sd_ssd_mobilenet_v1 model on my own dataset but only after adding more data to my original dataset. Is there a lower limit to that? When I don't add more photos and annotations to my original dataset I get this:
FileNotFoundError: [Errno 2] Unable to synchronously open file (unable to open file: name = 'C:\Users\Haris\Desktop\stm32ai-modelzoo\object_detection\src\experiments_outputs\2024_11_06_16_14_16\saved_models\best_weights.h5', errno = 2, error message = 'No such file or directory', flags = 0, o_flags = 0)
Using chain_tqeb doesn't create a .tflite file which I believe is what is needed to download to the board, correct?
Don't we need to convert the .h5 file to .tflite?
I would then add my newly trained model to general.model_path in the .yaml file.
Please let me know. Really appreciate the much needed help so we can quickly go to developing a product with this.
thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-07 7:32 AM
Hello @dogg ,
I don't know about a lower limit concerning data, I will ask the dev team.
Concerning the quantization, if everything went correctly, you should have a .tflite model in /experiment_output/<date of experiment>/quantized_model.
You can try to use only the quantization operation mode:
- Add a quantization path in the dataset part of the yaml, it is advised to put the training data.
- You may need to use the model_path in the general part and comment everything from training/model:
general:
project_name: COCO_2017_person_Demo
model_type: st_ssd_mobilenet_v1
model_path: <PATH TO YOUR TRAINED MODEL>
logs_dir: logs
saved_models_dir: saved_models
gpu_memory_limit: 12
global_seed: 127
operation_mode: quantization
training:
# model:
# type: st_ssd_mobilenet_v1
# alpha: 0.25
# input_shape: (256, 256, 3)
# weights: None
# pretrained_weights: imagenet
...
Leave everything else the same.
If it doesn't work, you can also try to use the ST Edge AI Dev cloud to do the quantization instead of the local installation of ST Edge AI. Just change on_cloud to True. (you need a st accound and you will be ask to log after running the python script)
tools:
stedgeai:
version: 9.1.0
optimization: balanced
on_cloud: True
path_to_stedgeai: C:/Users/haris/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/9.1.0/Utilities/windows/stedgeai.exe
path_to_cubeIDE: C:/ST/STM32CubeIDE_1.16.1/STM32CubeIDE/stm32cubeide.exe
Finally, if it does not work, you can also quantize it manually on the ST Edge AI Dev Cloud
Documentation: https://wiki.st.com/stm32mcu/wiki/AI:Getting_started_with_STM32Cube.AI_Developer_Cloud
Let me know if it helps.
Julian
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-07 7:42 AM
Hello dogg,
There are many aspects in your question.
There is a simple service to convert a h5 model to TFLite
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-08 12:49 AM - edited ‎2024-11-08 1:44 AM
Hi,
Thanks for the info.
I did find the .tflite file inside quantized_models...
I have one more question for now and I will open a different thread if I stumble on something else in the process.
How can I use my nvidia gpu for the training with this script?
This is a bit confusing to me:
thanks