2024-07-05 06:39 AM - edited 2024-07-05 07:10 AM
Why does the datalogger crash when I put a device_config.json file on the SD card ?
I created the device_config.json file using the Python GUI tool, saved it to the computer and then copied it to the root folder of the SD card.
The only changes I made was to the accelerometers where I changed the range to 4g (with the exception of IIS2ICLX which was left at 3g).
I put the SD card in the STWINBX1 and pressed the RESET button.
When I try to start the log (by pressing the USER button) the software seems to crash.
The green LED (LED_1) stays in the state when the USER button was pressed (i.e. permanently on or off).
The board has to be reset, but then the same happens again if I try to start a log.
When I try to access the log files on the SD card on the computer, I get an error saying the directory is corrupt, so this probably shows that the software is crashing...
I cannot delete the folders, so I have to reformat the SD card.
I have attached a copy of the device_config.json file (note I had to rename the extension to .txt in order to attach).
Solved! Go to Solution.
2024-07-17 02:41 AM
Hello @johngj
I confirm that I found and fixed the issue in the FW. v2.2.0 will work as expected.
As described in the User Manual, we suggested some SD card part number that we fully tested. We can't guarantee that any kind of SD card can support the amount of data we are logging.
The manual contains also a detailed explanation for the SD card failing and a procedure to test your SD card if you still don't want to use one of the suggested ones.
Best regards
Simone
2024-07-08 12:41 AM
Hello @johngj
I'll replicate your setup to find the issue. For sure, I'll integrate the bugfix in the upcoming FP-SNS-DATALOG2 v2.2.0.
In the meantime, which sd card are you using? FP-SNS-DATALOG2 User Manual includes a list of tested and suggested sd card part number and a troubleshooting paragraph.
Best regards
Simone
2024-07-10 08:42 AM
The SD card is a 2GB Transcend card, part number TS2GUSD...
https://uk.rs-online.com/web/p/sd-cards/1871643
https://docs.rs-online.com/3ea7/0900766b816fae97.pdf
2024-07-17 02:41 AM
Hello @johngj
I confirm that I found and fixed the issue in the FW. v2.2.0 will work as expected.
As described in the User Manual, we suggested some SD card part number that we fully tested. We can't guarantee that any kind of SD card can support the amount of data we are logging.
The manual contains also a detailed explanation for the SD card failing and a procedure to test your SD card if you still don't want to use one of the suggested ones.
Best regards
Simone
2024-07-18 01:11 AM
When will FW. v2.2.0 be released ?
To clarify, the SD card seems to work fine.
The problem only occurs when I put a device_config.json file on the SD card root folder.
It sounds like you found a bug and have fixed this in FW. v2.2.0 ?
2024-07-19 01:05 AM
Hello @johngj
v2.2.0 should be online in a couple of weeks, and it will fix your issue.
Best regards
Simone