cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6

AMend.7
Associate III

Hi,

When ST will release more information about the STM32N6? Will it use the new cortex-m55? Can it be used in motor control applications?

13 REPLIES 13
ramil
Associate II

Hello @Miguel CASTRO,

It's been a while since the last update. Are there more details about the product and when it will be released? 

Thank you, 

Ramil

Hi @ramil ,

 

despite there is still no official announcement it is already available in the latest software updates (Cube and CubeIDE). Shortly:

  • M55 (with Helium I guess) at 800MHz
  • 4MB RAM, no internal flash
  • Rich in connectivity: 3xFDCAN, ETH, 2xSDMMC, 2xUSB OTG HS
  • Rich in multimedia (CSI, DCMI, GPU2D)
  • VFBGA only

 

Regards,

Dmitry

Hello everyone,

 

I highly suggest you attend to the ST32 Summit on the 10th to the 13th of December and in particular, to register for the events on the 12th and 13th as they are dedicated to AI accelerated hardware and AI software solution

STM32 Summit - STMicroelectronics

 

Have a good day,

Julian

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @DmitryR ,

The STM32N6 has been officially launched yesterday at the STM32 Summit !

Please refer to the following post for more details on the full AI ecosystem and useful links:

STM32N6 has been officially launched - STMicroelectronics Community

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen