cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 and X-CUBE-AI problems: "TOOL ERROR: List index out of range"

AM-adben
Associate II

Hello,

I am facing some strange errors when trying to analyze any TFLite model. The errors are occurring in the following situations:

Situation 1: STM32Cube.AI MCU Runtime

When analyzing a TFLite model, it fails and shows an error message: "TOOL ERROR: List index out of range."

1.png

Situation 2: STM32Cube.AI Neural-ART Runtime

After clicking on the Analyze button, it's stuck at 0%. Nothing else happens, even after I wait for 30 minutes.

2.png

I am using:

CubeIDE version: 1.17.0
X-CUBE-AI version: 9.0.0 and 9.1.0

Please note that all those TFLite models work fine with CubeIDE 1.16.0, X-CUBE-AI 9.0.0, and STM32H7A3.

I am attaching 2 tflite models for your reference.

1 ACCEPTED SOLUTION

Accepted Solutions
hamitiya
ST Employee

Hello @AM-adben ,

Could you please verify again your version of X-CUBE-AI ?

Neural-ART Runtime should only be available from X-CUBE-AI version 10.0.0.

Did you install the runtime through STM32CubeMX or STEdgeAI-Core installer ?

 

My first suggestion would be to uninstall X-CUBE-AI through STM32CubeMX, and install it again. After that, verify the content available in C:\Users\your_username\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0.

You should have this file tree:

hamitiya_0-1736839842963.png

 

Best regards,

Yanis

 

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
hamitiya
ST Employee

Hello @AM-adben ,

Could you please verify again your version of X-CUBE-AI ?

Neural-ART Runtime should only be available from X-CUBE-AI version 10.0.0.

Did you install the runtime through STM32CubeMX or STEdgeAI-Core installer ?

 

My first suggestion would be to uninstall X-CUBE-AI through STM32CubeMX, and install it again. After that, verify the content available in C:\Users\your_username\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0.

You should have this file tree:

hamitiya_0-1736839842963.png

 

Best regards,

Yanis

 

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Sorry for the late reply as I was on leave.

I installed X-CUBE-AI version 10.0.0 which was not availabe in CubeMX earlier when I made this post. Anyway, now I can analyze the model using "STM32Cube.AI MCU Runtime" option. But, "STM32Cube.AI Neural-ART Runtime" requires STEdgeAI-NPU package which I don't have access to. I requested for this package earlier. Today I requested again. Without it, I can't use the NPU.

Hello @AM-adben 

You are right, STEdgeAI-NPU package is required in order to use Neural-ART Runtime. 

If the request was done more than 2 days ago, could you please check in your mailbox if this mail did not go in spam folder ?

 

Best regards,

Yanis

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks! The mail was indeed in spam.

I downloaded it and "analyze" using STM32Cube.AI Neural-ART Runtime worked fine. I am yet to run the model though.

Thank you for your assistance.