cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeAI BUG

奥特曼9527
Associate II

Hi,

Every time I click on the AI model, my clock tree is forcibly changed, and the external clock is also changed for me.

9527_0-1741926220317.png

9527_1-1741926246640.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
hamitiya
ST Employee

Hello,

Yes some parameters are defined as "required" and they apply at X-CUBE-AI launch.

The prompt you saw is only about "optimal parameters".

If you want to disable this behavior, here is the following:

- Open $HOME\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0\db\boardExternalMem.xml (Windows HOME equivalent is C:\Users\<username>)

- Find your Discovery Kit board or your Die ID (Example: STM32F746G-DISCO is die 0x449)

- Remove or comment the lines in object "requiredParameters"

 

Best regards,

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
奥特曼9527
Associate II

Has no one encountered this problem? Is there no expert using this thing?

hamitiya
ST Employee

Hello,

Yes some parameters are defined as "required" and they apply at X-CUBE-AI launch.

The prompt you saw is only about "optimal parameters".

If you want to disable this behavior, here is the following:

- Open $HOME\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0\db\boardExternalMem.xml (Windows HOME equivalent is C:\Users\<username>)

- Find your Discovery Kit board or your Die ID (Example: STM32F746G-DISCO is die 0x449)

- Remove or comment the lines in object "requiredParameters"

 

Best regards,

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

9527_0-1742478439848.png

Note that when I modify my hardware configuration, the external crystal oscillator is 25M and it changes to 8M every time I click on it. Your software forces it to be 8M. 

9527_1-1742478843087.png

These generated file paths are also missing some things and have to be changed every time. The library files have to be deleted manually every time.