2020-07-04 4:13 AM
Hi All,
I am developing product using LSM6DSOX and plan to use MCL for classification. Current process of development is following:
1 gathering raw data
2 generating ARFF file with features using Unico GUI
3 generating decision trees using our py code
4 generate MLC configuration using Unico GUI
I want to void Unico GUI on second step. Do you have python or any other language libraries to generate ARFF file with features?
As for 4th step, as I understood MLC configuration can be done only in Unico GUI. Is it possible to run it in shell mode? The reason that I want to make precess seamless and as less as possible related to user-driven actions.
2020-07-06 3:17 AM
Hi @VNero.1 , please check private correspondence. Regards
2021-02-28 6:36 PM
@Eleon BORLINI Please let me know what is the answer.
2021-03-01 1:00 AM
Hi @MLaza.1 ,
we have internal code available but it's not open source.
For this reason, you should contact our Sales and representatives or our OLS from the st.com webpage, so that they can evaluate case by case and eventually give you the code python code after signing the LUA.
-Eleon