cancel
Showing results for 
Search instead for 
Did you mean: 

Can we program MLC without ST apps or without ST development boards?

Evelina CAMILLERI
ST Employee

 [webinar - Program decision trees in sensors with a Machine Learning Core]

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Evelina CAMILLERI
ST Employee

The Machine Learning Core (MLC) configuration has to be created with the Unico GUI, since it contains all the specific hardware settings of the ST devices. Unico GUI can also run offline, in order to create a configuration even without any ST development board connected to the PC. 

Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on ST sensors featuring the MLC capability as shown by the example available on the ST GitHub repository

View solution in original post

1 REPLY 1
Evelina CAMILLERI
ST Employee

The Machine Learning Core (MLC) configuration has to be created with the Unico GUI, since it contains all the specific hardware settings of the ST devices. Unico GUI can also run offline, in order to create a configuration even without any ST development board connected to the PC. 

Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on ST sensors featuring the MLC capability as shown by the example available on the ST GitHub repository