2024-01-25 11:56 PM
Hi ST professional team
Following the documentation instructions & opterating
How to resolve compilation error messages:
Solved! Go to Solution.
2024-01-26 12:48 AM
Hello @cvd_pony and welcome to the STM32 Community :)
Check your builder settings.
Make sure to configure your project properly and build the workspace in the right path.
2024-01-26 12:48 AM
Hello @cvd_pony and welcome to the STM32 Community :)
Check your builder settings.
Make sure to configure your project properly and build the workspace in the right path.
2024-01-26 1:46 AM
I'll try it, thank you
2024-01-29 5:49 AM
I did the Wiki again on my side and did not face any issue.
For your case and would verify two steps :
Delete the following files and replace them with the ones from workspace/stm32ai_output:
In Src:
In Inc:
FP-AI-VISION1 v3.1.0 is based on X-Cube-AI version 7.1.0, You can check your version of Cube.AI by running stm32ai --version. If the c-model files were generated with a newer version of X-Cube-AI (> 7.1.0), you need also to update the X-CUBE-AI library (NetworkRuntime720_CM7_GCC.a for X-CUBE-AI version 7.2).
Go to workspace/FP-AI-VISION1_V3.1.0/Middlewares/ST/STM32_AI_Runtime then for a Windows command prompt:
copy %X_CUBE_AI_DIR%\Middlewares\ST\AI\Inc\* .\Inc\ copy %X_CUBE_AI_DIR%\Middlewares\ST\AI\Lib\GCC\ARMCortexM7\NetworkRuntime720_CM7_GCC.a .\lib\NetworkRuntime710_CM7_GCC.a
2024-03-26 4:46 AM
Hi,
I had a similar problem when following the tutorial above, as well as this one:
How to use transfer learning to perform image classification on STM32
Specifically, I got a linker error saying that some function related to NT35510 could not be found (some file names are removed):
undefined reference to `NT35510_RegisterBusIO'
undefined reference to `NT35510_ReadID'
in function `BSP_LCD_InitEx':
undefined reference to `NT35510_LCD_Driver'
collect2.exe: error: ld returned 1 exit status
I had followed the instructions in step 3.3 of the tutorial above (same as step 3.1.4 in the tutorial you mentioned) and moved the two files nt35510.c and nt35510_reg.c to the folder workspace/FP-AI-VISION1_V3.1.0/Drivers/BSP/Components, but the linker still didn't find them.
Solution: After a few hours of googling and trial and error, I realized that much of the project file tree is mirrored as a sub-tree of the STM32 project in the STM32Cube IDE file tree, and that I needed to drag and drop the two C-files into the sub-folder Components of the project tree. The image below shows the incorrect folder in red and the correct one in green:
I held the Ctrl key while dragging and dropping the files, to do a copy. I then got a dialog asking if I wanted to copy or link the files, and I selected linking. This seemed to update the build system so the files were included in the compilation, and solved the linking problem.
I think this should be updated in the instructions of both tutorials.
Hope it helps someone else!
2024-03-27 7:27 AM
Thank you Magnus,
you are right. This is the correct way of doing it.
I am reworking the wiki, to make it easier. Stay tune !
With Kind Regards,
Nicolas,