2024-04-16 3:51 AM - last edited on 2025-01-08 1:41 AM by SimonePradolini
Hi, I have a STEVAL-STWINKT1B that I am using to log data into my PC with HSDPython_SDK.
How can I set the accelerometer range (for example IIS3DWB to 16g)?
Regards,
Ivan
Solved! Go to Solution.
2025-01-08 1:48 AM
Hello @iarakis
Sorry for the late reply, I noticed your request just now.
HSDPython_SDK contains a GUI-based demo called hsdatalog_GUI.py. Have you ever used it?
Sensor parameters can be setup from the menu available on the left of the GUI.
Is this widget not working properly on your side? Which Python version are you using?
Best regards,
Simone
2024-12-10 5:26 AM
Hey, you can use the app "ST BLE Sensor" to connect to the STEVAL-STWINKT1B and change the parameters of the different sensors. In particular, you can change the full-scale parameter of the IIS3DWB sensor.
2025-01-08 1:48 AM
Hello @iarakis
Sorry for the late reply, I noticed your request just now.
HSDPython_SDK contains a GUI-based demo called hsdatalog_GUI.py. Have you ever used it?
Sensor parameters can be setup from the menu available on the left of the GUI.
Is this widget not working properly on your side? Which Python version are you using?
Best regards,
Simone
2025-01-20 5:14 AM
Hello @iarakis
Is the issue solved? Can you provide us with feedback by accepting the solution or coming back to us with a further request?
Best regards,
Simone