cancel
Showing results for 
Search instead for 
Did you mean: 

Data log with STEVAL-STWINKT1B using HSDPython_SDK and set accelerometer range to 16g

iarakis
Associate II

Hi, I have a STEVAL-STWINKT1B that I am using to log data into my PC with HSDPython_SDK.

How can I set the accelerometer range (for example IIS3DWB to 16g)?

Regards,

Ivan

1 ACCEPTED SOLUTION

Accepted Solutions
SimonePradolini
ST Employee

Hello @iarakis 

Sorry for the late reply, I noticed your request just now.

HSDPython_SDK contains a GUI-based demo called hsdatalog_GUI.py. Have you ever used it?

Sensor parameters can be setup from the menu available on the left of the GUI.

SimonePradolini_0-1736329713193.png

Is this widget not working properly on your side? Which Python version are you using?

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3

Hey, you can use the app "ST BLE Sensor" to connect to the STEVAL-STWINKT1B and change the parameters of the different sensors. In particular, you can change the full-scale parameter of the IIS3DWB sensor.

SimonePradolini
ST Employee

Hello @iarakis 

Sorry for the late reply, I noticed your request just now.

HSDPython_SDK contains a GUI-based demo called hsdatalog_GUI.py. Have you ever used it?

Sensor parameters can be setup from the menu available on the left of the GUI.

SimonePradolini_0-1736329713193.png

Is this widget not working properly on your side? Which Python version are you using?

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @iarakis 

Is the issue solved? Can you provide us with feedback by accepting the solution or coming back to us with a further request?

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.