cancel
Showing results for 
Search instead for 
Did you mean: 

Calibrating LSM6DSOX in arduino nano rp2040

SRodr.4
Associate II

Hello,

I am doing a project for fall detectino using the MLC in the LSM6DSOX. However, i noticed that the output of the sensor for the accelerometer show values on the 1000 mg range for the z axis. I would like to calibrate the sensro but the only way I found to do this is using the Motion_AC library. However, I don't know how I could use this library in the Arduino environment and more precisely for the board Nano RP2040 connect. Does anybody know how to perfomr the calibration?. Thanks.

2 REPLIES 2
SRodr.4
Associate II

The main issue is I want the calibrated values to go into the MLC for classification. I could use a general code for calibration but I need the calibrated values from the accelerometer to go into the MLC.

Federica Bossi
ST Employee

Hi @SRodr.4 .

 

Why do you want to do a calibration? 1000mg on the Z axis is expected.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.