2023-07-12 02:15 AM
Hello every Body, i am investigating the use of ISM330IS with nanoEdgeAI to detect Anomaly situations.
Lets take a motor for air conditioning as an example, If the motro has protection against high current, and a tachometer, What are the benefits of ISPU against those typical protection.
the seconde question is ,is there any industrial project using the ISPU to detect anomality ?
thank you very much
Solved! Go to Solution.
2023-07-12 11:50 PM
Hi @M.Mardini ,
when you use ISPU to detect anomalies, you are searching for differences in the movements between the normal functioning of the device and a faulty one. This means that you can also manage to detect a problem that the other two methods are not able to detect, like a strange movement on one of the axis.
at the moment, there are no industrial project available, but I think there are people already working on it =)
Niccolò
2023-07-12 11:50 PM
Hi @M.Mardini ,
when you use ISPU to detect anomalies, you are searching for differences in the movements between the normal functioning of the device and a faulty one. This means that you can also manage to detect a problem that the other two methods are not able to detect, like a strange movement on one of the axis.
at the moment, there are no industrial project available, but I think there are people already working on it =)
Niccolò