2021-03-23 03:28 AM
2021-03-23 09:04 AM
Hello @ShivaRagu ,
Thanks for your feedback
If I well understand your problem, you cannot uninstall the STM32CubeMX tool from your machine, which is a bit odd since CubeMX can be successfully installed and uninstalled.
Please refer to the STM32CubeMX Reference Manual, the 3.2 Installing/uninstalling STM32CubeMX standalone version section details multiple methods to complete the uninstall process.
Hope this resolve your issue.
Khouloud.
2021-03-24 05:21 AM
2021-03-24 01:05 PM
Hi @ShivaRagu ,
Let me share with you my comprehension to avoid any misunderstanding: so, you have downloaded FP-AI-SENSING1 pack and you browse the Session_keras_mod_93_Model.h5 keras model after enabling the Artificial Intelligence search criteria in the MCU selector tab. Did I correctly reproduce your scenario?
Actually, following the steps above, no error window is displayed and the file is analyzed without any problem:
Could you please precise which CubeMX version are you using ?
Also, you can attach your log files under: <USER_HOME>\.stm32cubemx\STM32CubeMX.log and <USER_HOME>\.stmcufinder\STMCUFinder.log. They may revel the root cause of this misbehavior.
Thanks in advance.
Khouloud.
2021-03-24 10:39 PM
Hi Gm,
I installed the latest version of stm32cubemx V 6.2.0 and also enabled the AI (latest version). I don't know why am getting error while uploading .h5 file.
Am not able to analyze the model. Is there any version problem in mx. May be if i try some older version will it work?
Regards,
shankari.