2020-02-07 1:22 AM
Although SPC582B family has up to 7 FlexCAN modules, some units have only 3 (i.e. SPC582B60E1CD00X).
Which 3 of 7 CAN modules are available in this processor?
Since SPC5Studio shows 7 CANbuses for this processor, I don't know which I/O should I design for CANbuses.
Solved! Go to Solution.
2020-05-08 3:52 AM
This information will be published in DS rev4
2020-02-07 6:21 AM
Yes , in SPC5Studio , we are seeing 7 Can Buses
You can use the Pinmap Wizard in order to determine which I/O Buses are designed for CAN Bus
It is very useful.
I am checking in the RM.
and check with experts
Best regards
Erwan
2020-02-07 8:27 AM
Unfortunately, in this case, I cannot use SPC5Studio to see which I/O pins are designed for CANbus in SPC582B60E1CD00X.
SPC5Studio shows that this processor has 7 CANbuses, while actually it has only 3.
In SPC5Studio there is no choice between SPC582B60E1CD00X (3 CANbuses) and SPC582B60E1MH00Y (7 CANbuses):
Waiting for the answer from experts :)
Yannek
2020-02-07 9:00 AM
I bet you get the information faster from datasheet of the given mcu.
2020-02-07 9:20 AM
I bet you don't, JoniS. Not only faster. Not at all.
2020-02-12 7:32 AM
Hi Erwan,
Would you have any information in this topic, please?
Our project stucked, because we don't know which pins should be used...
Best,
Yannek
2020-05-08 3:52 AM
This information will be published in DS rev4