cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5Studio (V3-V2) Can not Code Generated for SPC560Bxxx

orhanyilmaz
Associate II
Posted on June 11, 2014 at 14:55

Hello,

I'm trying to create new project (Starting Code Generating) with SPC5 Studio Version (2 or 3) for SPC56B/Cxx Series. But It doesn't generated. SPC5 Console Out:

Begin processing component resource com.st.tools.spc5.components.platform.spc560bcxx_1.0.0.201405131114/component/root_wo/
> Processing main.c
> Processing debug.wsx
> Processing stm_xpc560b_minimodule_debug_jtag.cfg
> Processing user.mak
Begin processing component resource com.st.tools.spc5.components.platform.spc560bcxx_1.0.0.201405131114/component/root_wa/
> Processing application.ld.ftl
Error: Expression conf.instance.runtime_settings.irq_stack_size.value[0] is undefined on line 28, column 29 in application.ld.ftl.
Error: FMPP processing session failed.
Error: An error occurred while generating component SPC560B/Cxx Platform Component
Begin processing component resource com.st.tools.spc5.components.platform.spc560bcxx_1.0.0.201405131114/component/cfg/
> Processing boot.h.ftl
> Processing platform.h.ftl
Begin processing component resource com.st.tools.spc5.components.platform.spc560bcxx_1.0.0.201405131114/component/mak/
> Processing component.mak.ftl
Begin processing component resource base files
> Processing components.c.ftl
> Processing components.h.ftl
> Processing components.mak.ftl
----------------------------------------------------------------------------------------------------
Application Generation Summary
----------------------------------------------------------------------------------------------------
SPC560B/Cxx Platform Component ...ERROR!

What should I do? #code-generate-error #spc5studio #irq-stack-size-error
This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
orhanyilmaz
Associate II
Posted on June 12, 2014 at 18:24

Hello Erwan,

Yes! Good news. but,

What should I do? :) (Patch etc.)

Best Regards

Orhan YILMAZ

Have a nice day. ;)

Erwan YVIN
ST Employee
Posted on June 13, 2014 at 10:04

Hello orhan ,

in SPC5Studio 3.0, we are calling toLower from String class, and this depends on the locale.

The toLower method comments are:

/**

     * Converts all of the characters in this

<code>

String

</code>

to lower

     * case using the rules of the default locale. This is equivalent to calling

     *

<code>

toLowerCase(Locale.getDefault())

</code>

.

     *

<p>

     *

<b>

Note:

</b>

This method is locale sensitive, and may produce unexpected

     * results if used for strings that are intended to be interpreted locale

     * independently.

     * Examples are programming language identifiers, protocol keys, and HTML

     * tags.

     *

For instance,

<code>

''TITLE''.toLowerCase()

</code>

in a Turkish locale

     * returns

<code>

''t\u0131tle''

</code>

, where '\u0131' is the LATIN SMALL

     * LETTER DOTLESS I character.

     * To obtain correct results for locale insensitive strings, use

     *

<code>

toLowerCase(Locale.ENGLISH)

</code>

.

     *

<p>

     *

@return

  the

<code>

String

</code>

, converted to lowercase.

     *

@see

     java.lang.String#toLowerCase(Locale)

     */

   

public

String toLowerCase() {

       

return

toLowerCase(Locale.getDefault());

   

}

       We will ping you and implement a patch by update site.

       Please check your mail.

 

Best regards

                   Erwan YVIN

Erwan YVIN
ST Employee
Posted on June 13, 2014 at 10:23

Re orhan ,

When the patch will be ready 

Help ==> Install New Software

Click on 

SPC5Studio - http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio_Update_Site

and update all the features.

Best regards

Erwan

orhanyilmaz
Associate II
Posted on June 13, 2014 at 10:45

Hello Erwan,

I'm trying update. Screen out adding. Not new update..

Best Regards

Orhan YILMAZ

________________

Attachments :

screen2.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qXGt&d=%2Fa%2F0X0000000boj%2FSMDzCTURMbieMPLkJe7VmH4vi9xDhYPwKWU9ZlNppTo&asPdf=false
Erwan YVIN
ST Employee
Posted on June 16, 2014 at 17:40

Thank you for your positive feedback ;)

The new SPC5Studio core version has been submitted in the official update site to correct the string class issue :

http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio_Update_Site

  Best regards

                  

                  Erwan

orhanyilmaz
Associate II
Posted on June 17, 2014 at 07:16

Hello Erwan,

Thanks for your help.

Have a nice day.

Best Regards

Orhan YILMAZ