cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560P44L3 Center alignment PWM generation.

RRama.3
Associate

Controller: SPC560P44L3 (Custom board)

IDE: SPC Studio

Im facing problems in generating 16kHZ frequency PWM center alignment.

For frequencies below 500Hz I was able to generate PWM center alignment, as per the code generation settings. But going for higher frequencies above 1kHz I see that alignment miss matches.

Please do find the attached code for the reference.

Thank you in advance.

0 REPLIES 0