cancel
Showing results for 
Search instead for 
Did you mean: 

i can't receive multiple data in lin slave mode

PLEE.2
Associate II

SPC58EC80E1 is used and only lin slave mode is used.

So, in the example code (SPC58ECxx_RLA LIN Test Application for Discovery), delete the lin_lld_start (&LIN_MASTER....) corresponding to the master and activate only lin_lld_start (&LIN_SLAVE...).

and then,​

If i send data (id+8bytes: 0x3c, 0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18) from the external device (PEAK-LIN) to the board, slave_rx_callback is called, but idMessage (0x3C) is received, but buffer is received only 1byte (0x11) and after 2bytes is received 0x00, 0x00 .....)

​

I wonder if spc5xx_lin_rxi_interrupt should be modified or what settings should be set when initializing.

​

LIN Configuration Setting of SPC58ECxx Low Level Drivers Component RLA is set to Synchronous 

and LIN_SLAVE set LD1

And.

Slave_tx_callback seems to be operated by the master function of the sample code.

I want to send the data to the master of the external device after slave_rx_callback.

I want to know how to call save_tx_callback. 

thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ODOUV.1
ST Employee

Hello,

thank you for your findings, I will forward to R&D team.

Best regards.

PLEE.2
Associate II

problem solved