2022-04-06 4:53 AM
I am using SPC58EC. When I compile same code with GNU and GHS(Green Hills Software) I see different results.
int main(void) {
uint8_t mode;
MC_ME.PCTL[15].R = (uint8_t)18;
mode = (uint8_t)MC_ME.MCTL.B.TARGET_MODE;
//SPCSetRunMode
/* Clearing status register bits */
MC_ME.IS.R = 0x3FU;
/* Starts a transition process.*/
MC_ME.MCTL.R = (mode << 28) | 0x5AF0UL;
MC_ME.MCTL.R = (mode << 28) | 0xA50FUL;
/* Waits for the mode switch or an error condition.*/
while (MC_ME.IS.R == 0U) {
;
}
/* Check if no error during mode switch */
if (MC_ME.IS.B.I_MTC != 1U)
{
while(1);
}
SIUL2.GPDO[88].R = 0;
SIUL2.MSCR_IO[88].R = ((2 << 24) | (1 << 23));
SIUL2.GPDO[89].R = 0;
SIUL2.MSCR_IO[89].R = ((2 << 24) | (1 << 23));
/* Application main loop.*/
for ( ; ; ) {
SIUL2.GPDO[88].R = ~SIUL2.GPDO[88].R;
SIUL2.GPDO[89].R = ~SIUL2.GPDO[89].R;
for(long i=0;i<10000000;i++);
}
}
All code is this, I am not using library functions. Startup files are almost same only order of ram init, interrupt vector init etc. is different. In GNU version I can toggle LED, but in GHS version I cant modify SIUL2 registers, so I cant do settings or toggle the output. Why is this happening? Cant we compile SPC5 studio example codes with GHS?
Solved! Go to Solution.
2022-04-08 5:43 AM
I removed that part and it is still working, anyways thank you for your help.
2022-04-08 5:52 AM
Hello,
it concludes it is not the root cause of your issue.
I wonder if you have the same definition of SIUL2 in your 2 projects ?
on SPC58EC it should be:
#define SIUL2 (*(volatile struct SIUL2_tag *) 0xf7fc0000UL)
BRs,
-Olivier
2022-04-08 6:10 AM
Yes those definitions are same. As I said I commented out existing project's code and used the code above only toggling LEDs. It didn't work so I gave up commenting out their initialization and use it. I only put this part:
SIUL2.GPDO[88].R = 0;
SIUL2.MSCR_IO[88].R = ((2 << 24) | (1 << 23));
SIUL2.GPDO[89].R = 0;
SIUL2.MSCR_IO[89].R = ((2 << 24) | (1 << 23));
That way let me change SIUL2 and I could toggle LEDs. I couldn't understand because assembly codes of main functions were same, so code was trying to modify that register and processor doesn't let it change. Also in debug session I couldnt change it from SFRs window. It somehow does protection or something like that.
2022-04-08 9:40 AM
As you removed all ST libraries, I wonder if you also removed the stuff done at boot in clock.c
void __early_init(void) {
spc_clock_init();
}
removing that, I cannot toggle the led either.
BRs,
-Olivier
2022-04-08 10:08 AM
I am so sorry, I didn't see it was weak function and __early_init name was like just assembly function, I couldn't imagine ST define it in .c file so I didn't even search in project. I only looked in that file and __early_init was an empty function. Thank you for making me awake to this and thank you for all replies and support.
2022-04-11 12:54 AM
Thank you for your answer.
Happy that the situation is unlocked at your side.
Best regards,
-Olivier