2020-01-08 08:47 AM
Hello
I am looking for a library and/or code examples of DSP and mathematical functions using the SPE for speed optimization. The one referred in ST is discontinued and not available.
Thanks in advance.
caio@canoo.com
Solved! Go to Solution.
2020-01-14 07:54 AM
Hello ,
For which family ?
in the SPC5Studio tools suite ,
there is no example of DSP
except : SPC560Dxx OS-Less Math Library Test Application for Discovery
Some example Crypto application is enabling SPE
Best Regards
Erwan
2020-01-14 07:54 AM
Hello ,
For which family ?
in the SPC5Studio tools suite ,
there is no example of DSP
except : SPC560Dxx OS-Less Math Library Test Application for Discovery
Some example Crypto application is enabling SPE
Best Regards
Erwan
2020-01-14 09:59 AM
Hello Erwan
Thanks for the answer. I talked with someone in ST and the document where they refer to the examples and code was outdated and the library is/was not available. They are going to delete the reference to avoid further confusion.
Best of all
C.