Skip to main content
Associate III
November 18, 2023
Solved

Autodevkit 2.2 CAN Examples missing, version bug

  • November 18, 2023
  • 1 reply
  • 2046 views

I uninstalled my prior Autodevkit 2.1 which seemed to had a lot of trouble with my workspace. 

The new 2.2 looked promising. A minor bug is that it still shows 2.1 in the About/help section as in the release notes, as on the linked website of the release notes. 

 

But most disturbing: I miss my examples from the application library! If I choose AEK-MCU-C2MLIT1 or SPC58EC I cant see any CAN example. Even if i filter for CAN I get some results of which some dont even contain any CAN. 

The RLA CAN Test Application for discovery is gone (I used it on 2.1), I can find it when I select SPC58x Gxx - which does not work (UDE can´t get contact and load this onto the board) 

I also can´t find a example update function or release note what the examples are doing in particular or which UM/release note may walk me through them. How is the usage intended? 

This topic has been closed for replies.
Best answer by Max VIZZINI

Attached you can find the CAN RLA example to be imported.

Unzip it and put it in a working folder or AutoDevKit workspace folder.

Go to File>Open projects from File System

2023-11-19 16_47_48-workspace - AutoDevKitStudio.png 

Generate and compile the code.

I have also attached a PDF document with basic explanation on CAN usage.

Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
November 19, 2023

Attached you can find the CAN RLA example to be imported.

Unzip it and put it in a working folder or AutoDevKit workspace folder.

Go to File>Open projects from File System

2023-11-19 16_47_48-workspace - AutoDevKitStudio.png 

Generate and compile the code.

I have also attached a PDF document with basic explanation on CAN usage.

Regards,

AutoDevKit Team