cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the path of the spc5studio header file

WMa.2
Associate II

0693W00000WKWlRQAX.pngWhy can't I include the system standard header files? Why can I generate files even if there are problems as long as the console is fine when compiling? Finally, I can burn the program into the chip and run it successfully.0693W00000WKWlHQAX.png0693W00000WKWl2QAH.png0693W00000WKWkxQAH.png0693W00000WKWgbQAH.png0693W00000WKWgWQAX.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee

Dear Sir,

These standard types include are not needed because they are managed internally by SPC5Studio to deal with different compilers and to comply to MISRA rules.

In addition, anything is under the source folder in the project is compiled.

Finally, you can change compiling and linking options from the configuration of the platform.

Best Regards,

AutoDevKit Team

View solution in original post

1 REPLY 1
Max VIZZINI
ST Employee

Dear Sir,

These standard types include are not needed because they are managed internally by SPC5Studio to deal with different compilers and to comply to MISRA rules.

In addition, anything is under the source folder in the project is compiled.

Finally, you can change compiling and linking options from the configuration of the platform.

Best Regards,

AutoDevKit Team