cancel
Showing results for 
Search instead for 
Did you mean: 

Want to know about Software, Flash tool, Debug Tool required for AEK-AUD-CD-C1D9031

shiva_shankar_e
Associate II

Hi,

we want to know about AEK-AUD-CD-C1D9031. and Software, Flash tool, Debug tool. required for the AEK-AUD-CD-C1D9031.

As of now, for our present projects we are using 1) Cross Core Embedded Studio Development Environment (2.9.0) and 2) IAR Embedded Workbench for ARM (9.30.1).

and for Flashing of hex file we are using ' ICE1000 ' and ' IAR I-jet '.

can you suggest any thing that we can Reuse from Present Project. or we have to buy set of new things.

1 REPLY 1
Max VIZZINI
ST Employee

Hi,

The supported tool chain are:

- OpenOCD (only in latest version of AutoDevKit Studio www.st.com/autodevkitsw )

- PLS UDE

The first is completely free while the second is free for code download up to 256K. 

Please note that the above two programmer/debugger are incompatible with each other, therefore cannot be both installed on your PC.

Best Regards,

AutoDevKit Team