cancel
Showing results for 
Search instead for 
Did you mean: 

FAD903D volume control

shiva_shankar_e
Associate III

hi community 

i am using  "AEK-AUD-C1D9031"  board. in this board i had flashed  .WAV files and i had played. the wave files are played using an example code given in the autodevkit. i used an API playsound() this one will give good sound when i had used playsoundwithgain() -> the gain with range (15,17) the sound quality was good with decent amount of volume. but hear i want to control the volume  (0db - 75db),but by using playsound() and playsoundwithgain() i am unable to control the volume( the sound will be very noise when i had used gain in range of ( (0-14) and (17- so...on) ). so is there any alternatives to control the volume of the sound.

 

hear is the pic of the function which i had used.image.png

0 REPLIES 0