2023-08-07 12:21 PM
Hi,
I just moved from stm32 with Cube IDE into AutoDevKit with an AEK-MCU-C4MLIT1 discovery board.
I am so frustrated after a complete 8 hour spin and still no results.
Why is AutoDevKit called an IDE when the Debugger is still external? I dont get it.
I tried to get it running and found posts heer, 3 years old already stating that the eclipse integration tool does not work anymore.
I run into trouble with the external UDE debugger as well, plenty of them.
Is there an IDE as CUBE where I can get everything for the SPC controllers? Is there an explanation and code example of simple things like blinking LEDs, hello word kind of things? Or is there a way to run SPC58 in CubeIDE? Tips, suggestions?
Solved! Go to Solution.
2023-08-16 01:51 AM
Hello ,
You can not compiled SPC58 in CubeIDE ?
but you can install OpenOcd in AutodevKit Studio or SPC5Studio by using update site mecanism :
or
Install PLS Integrated debugger
http://spc5tools.spc5studio.com
Openocd (Linux/Windows) with eclipse plugins have a better integration in SPC5Studio/Autodevkit Studio than PLS (Windows only)
Best Regards
Erwan
2023-08-16 01:51 AM
Hello ,
You can not compiled SPC58 in CubeIDE ?
but you can install OpenOcd in AutodevKit Studio or SPC5Studio by using update site mecanism :
or
Install PLS Integrated debugger
http://spc5tools.spc5studio.com
Openocd (Linux/Windows) with eclipse plugins have a better integration in SPC5Studio/Autodevkit Studio than PLS (Windows only)
Best Regards
Erwan
2023-08-29 07:30 AM
Frankly, I am lost! I think the customers knowing how to manage all this don´t need the answer for the ones like me the common expectation is a double click on an exe file and maximum one additional driver for ftdi, the rest should just work.
2023-08-30 02:06 AM
STM32 (arm) has a greater community than SPC5 Family (powerpc) (more automotive part) but not the same bandwidth.
Same company but different IDE.
the good advantage of SPC5Studio / Autodevkit Studio (based on eclipse framework) , it is possible to install your own debugger and integrate it in your IDE. (like Cube)
I am here to help you
2023-11-18 07:19 AM
I have a bit of a hard time seeing how this is an advantage.
I do not have own debuggers, do not use Segger and so on. I would just expect that an IDE acts like an integrated development environment. Which means I press install and aftwards everything works. I hardly understand all of this Kludge, what is this?
Can´t I just get an out of the box working IDE with the drivers needed for the mcu/board?
A good documentation, libraries and all of this in one window?