cancel
Showing results for 
Search instead for 
Did you mean: 

If i buy BD 140 only- is it same with BD 140 -16 or BD 140- 10?

esisw.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @esisw.1​, to the community!

The pnp bipolar transistor BD140 will be supplied in three groups of the parameter hfe (see datasheet, page 4):

  • BD140: 40...250
  • BD140-10: 63...160
  • BD140-16: 100...250

Of course, it always depends on the circuit, but most of the time you can replace a BD140 with a BD140-10 or BD140-16, but not necessarily vice versa.

If you want to be sure that the circuit works safely with the BD140 instead of the BD140-10 or BD140-16, you have to measure the value of hfe of the BD140 and make sure that you are in the appropriate group with it.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @esisw.1​, to the community!

The pnp bipolar transistor BD140 will be supplied in three groups of the parameter hfe (see datasheet, page 4):

  • BD140: 40...250
  • BD140-10: 63...160
  • BD140-16: 100...250

Of course, it always depends on the circuit, but most of the time you can replace a BD140 with a BD140-10 or BD140-16, but not necessarily vice versa.

If you want to be sure that the circuit works safely with the BD140 instead of the BD140-10 or BD140-16, you have to measure the value of hfe of the BD140 and make sure that you are in the appropriate group with it.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Dear Mr Peter
Thank you for your information.
This answered my question.
Best regards
Edie S