2023-07-31 5:40 AM
Hello,
I found this link on the internet : https://github.com/logical/sgtl5000-stm42f4
But when i download and try to open it under STM32CubeIDE, I encounter errors such as this window.
Do you know how to convert to a correct format under STM32CubeIDE ? Thank you for your advice.
Regards.
2023-08-01 11:21 PM
2023-08-02 12:43 AM
The original project looks like for SW4STM32. Try to import is as SWSTM32.
2023-08-02 12:49 AM - edited 2023-08-02 12:50 AM
Hi,
Import under STM32Cube IDE ?
I have nothing about SWSTM32, do I have to download dedicated software for this project ?
2023-08-02 5:35 AM
Yes. In that menu, select "import acv6 System Workbench.... project"
2023-08-02 5:45 AM - edited 2023-08-02 5:46 AM
But, it's not complete, a lot of things are missing, for example the .ioc file
Probably I didn't do the right import method, I can't compile the project also.
2023-08-02 6:38 AM
Your RAR file doesn't include the whole project, just a few files. No chance of it working like that.
2023-08-02 6:43 AM
I couldn't get it to work either. You can always create a new project for the appropriate chip then replace all the files with the ones in your project.
2023-08-02 6:45 AM
Hi,
Sorry, in this forum I can't send a ZIP file (which contains all the files) and I converted the ZIP file to RAR online. That why missing files.
2023-08-02 7:23 AM
Why won't you contact the author of the github project. He may be glad to help.