cancel
Showing results for 
Search instead for 
Did you mean: 

How to import a project ?

DYann.1
Senior II

Hello,

I found this link on the internet : https://github.com/logical/sgtl5000-stm42f4

But when i download and try to open it under STM32CubeIDE, I encounter errors such as this window.

DYann1_0-1690807052162.png

Do you know how to convert to a correct format under STM32CubeIDE ? Thank you for your advice. 

Regards.

11 REPLIES 11
DYann.1
Senior II

Hello,

Here, you can find the project I don't know if it can open with STM32Cube IDE but I guess so. Thank you for your helps.

 

Pavel A.
Evangelist III

The original project looks like for SW4STM32. Try to import is as SWSTM32.

DYann.1
Senior II

Hi,

Import under STM32Cube IDE ?

DYann1_0-1690962462301.png

I have nothing about SWSTM32, do I have to download dedicated software for this project ?

Pavel A.
Evangelist III

Yes. In that menu, select "import acv6 System Workbench.... project"

But, it's not complete, a lot of things are missing, for example the .ioc file

DYann1_0-1690980250843.png

Probably I didn't do the right import method, I can't compile the project also.

TDK
Guru

Your RAR file doesn't include the whole project, just a few files. No chance of it working like that.

TDK_0-1690983526992.png

 

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Guru

I couldn't get it to work either. You can always create a new project for the appropriate chip then replace all the files with the ones in your project.

If you feel a post has answered your question, please click "Accept as Solution".

Hi,

Sorry, in this forum I can't send a ZIP file (which contains all the files) and I converted the ZIP file to RAR online. That why missing files.

Pavel A.
Evangelist III

Why won't you contact the author of the github project. He may be glad to help.