cancel
Showing results for 
Search instead for 
Did you mean: 

How to fix Noise issues in PDM to PCM Conversion?

AiROT
Associate II

Hey,

We are implementing digital microphone interfacing using ST's IMP34DT05TR microphones connected to the STM32G473VET6 microcontroller through the PDM interface, following guidelines from the application note AN5027, specifically Example 3.

The configuration includes:

1. SAI GPIO and Pin Configuration
2. SAI Parameter Settings
3. SAI DMA Settings

We have included screenshots of these configurations.

We are utilizing the PDM filter library "libPDMFilter_CM4F_GCC.a" for converting PDM to PCM. However, the output PCM data, when converted to a .wav file or played directly, results only in Noise.

Could you advise on what aspects to check or steps to troubleshoot this issue effectively? Any help or guidance would be greatly appreciated.

AiROT.

1 REPLY 1
PGump.1
Senior III

Hi,

Make sure the header in your WAV file is correct - sample rate, bit length, n channels, endiness...

I hope that helps.

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.