cancel
Showing results for 
Search instead for 
Did you mean: 

Issues with ST25DV04KC-IE8C3 NFC Chip Interference from Magnetic Switch

Nikunj_17
Associate III

Hello STM Community,

I'm currently working on a project involving the ST25DV04KC-IE8C3 NFC chip interfaced with the STM32L496ZG microcontroller. I've encountered an issue where the performance of the NFC chip deteriorates when a magnet is brought near the system, specifically related to the operation of a magnetic switch that generates interrupts.

Problem Description:

  • Components: The NFC chip is located approximately 3.6 mm away from a magnetic switch (RR132-2E32-551).
  • Issue: When the magnet is brought close to the magnetic switch, it appears to cause delays in counting and issues with I2C communication. Specifically, I suspect that the magnetic field is affecting the NFC chip's operation, leading to unexpected behaviour or interruptions that impact the STM32’s performance.
  • Effects on System:
    • Interruption in the NFC communication.
    • Possible noise was introduced on the I2C bus.
    • Delays in processing and timing, particularly in counting routines.

Troubleshooting Steps:

  • I’ve monitored the interrupt lines and found unexpected behaviour, suggesting that the magnet may be inducing noise or causing the NFC chip to misbehave.
  • I am considering moving the NFC chip to the bottom layer of the PCB and implementing shielding to mitigate the interference.

PCB Design:

I have attached a photo of the PCB layout for your reference. I would greatly appreciate any feedback on the design or suggestions on mitigating this issue!

Thank you for your assistance!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JL. Lebon
ST Employee

Hello, 

NFC is based on magnetic coupling between the reader and the tag. The reader is emitting a magnetic field at 13.56MHz that is captured by the tag's antenna, creating current into the antenna. Having a magnet nearby may disturb the magnetic field emitted by the reader.

Does the issue appear when there is a reader communicating with the tag and a magnet is put close to the switch? Or do you have issues when there is no RF reader in front of the tag?

Best regards.

View solution in original post

1 REPLY 1
JL. Lebon
ST Employee

Hello, 

NFC is based on magnetic coupling between the reader and the tag. The reader is emitting a magnetic field at 13.56MHz that is captured by the tag's antenna, creating current into the antenna. Having a magnet nearby may disturb the magnetic field emitted by the reader.

Does the issue appear when there is a reader communicating with the tag and a magnet is put close to the switch? Or do you have issues when there is no RF reader in front of the tag?

Best regards.