cancel
Showing results for 
Search instead for 
Did you mean: 

about TDA7492P burn

410791550
Associate
Posted on August 10, 2016 at 18:11

hi,

   I had some questions when i use the TDA7492P. When I turn on the 12V power(connect to the PVCC)and don't connect the 5V(connect to the SVCC), the pin1 of TDA7492P will

immediately

burn( the pin1 will short with pin2/pin3) .  I don't connect the L2~L9 and the

speaker。

    I had test 4pcs TDA7492P, they are all this case。

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nickname1623_O
Associate II
Posted on August 23, 2016 at 03:59

hi Ya dong ,

your application circuitry is wrong , SVCC must be connected with a capacitor between VSS. rather than external power supply .

please follow the application schematic in datasheet .

you can find it in below link.

http://www.st.com/content/ccc/resource/technical/document/datasheet/35/01/97/6b/20/ce/40/6f/CD00211320.pdf/files/CD00211320.pdf/jcr:content/translations/en.CD00211320.pdf

Thanks

YT