Associate III
February 10, 2025
Question
issues with a TD352
- February 10, 2025
- 6 replies
- 1957 views
Hi Everybody,
In the case of a LEDs tubes dimmer, I'm using a TD352.
It works very well. But in some case (and for the moment, I don't know why), my IGBT and the resistor wich controls the gate of the IGBT burn.
I just replace these two components and after it works well. It happens very rarely, but it happens.
IGBT can drive up to 80A (@ 25°C), and Vce is ok up to 650VAC, and the maximum inrush current that I measure is 35A, and the peak voltage, it's around 450VAC.
The value of the resistor is 51R in 0805 case.
The IGBT that I use is an IK40N65WR5.
If you have some suggestions to try to understand what happens, I'll be very happy.