STM32WB55 ADC Single scan (A/D9, A/D9, A/D10), using DMA AND LPTimer --- not seeing any values?
Good afternoon....
Trying to trigger scan mode (2 channels but 3 conversions ---- A/D 9, A/D 9, A/D 10) via software trigger that is called in the LPTIMER (I do not have access to other timers bcz they are tied up in other code that is why I am not using a trigger output) callback function. Can someone see something I am missing as the adcValue array is always empty ?
ADC CubeMx settings:
DMA CubeMx settings:
Main IRQ code: (In debugger I can see the timer running and I am getting to the Start DMA)
void HAL_LPTIM_AutoReloadMatchCallback(LPTIM_HandleTypeDef *hlptim)
{
if (hlptim == &hlptim1) //debounce timer
{
HAL_LPTIM_OnePulse_Stop_IT(&hlptim1);
if (HAL_GPIO_ReadPin(GPIOB, GPIO_PIN_1) == GPIO_PIN_RESET)
{
EXTI->PR1 |= EXTI_PR1_PIF1; //clear any that came AFTER debounce
EXTI->IMR1 |= EXTI_IMR1_IM1; //enable / unmask
ISR.B_LockOut = T;
}
}
else
{
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_4, 0); //LED on
// HAL_ADC_Start_IT(&hadc1);
hadc1.Instance->IER |= ADC_EOC_SEQ_CONV;
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adcValue, AD_NUMBERSAMPLES);
}
}
/*
* A/D conversion complete callback
*/
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
if (hadc == &hadc1)
{
// adcValue[cnt] = HAL_ADC_GetValue(&hadc1);
// cnt++;
// if ((hadc1.Instance->ISR) & 8UL)
// {
// HAL_ADC_Stop_IT(&hadc1);
HAL_ADC_Stop_DMA(&hadc1);
hadc1.Instance->IER &= ~ADC_EOC_SEQ_CONV;
hadc1.Instance->ISR |= ADC_EOC_SEQ_CONV;
// cnt = 0;
ISR.A_Conversion = T;
// }
}
}Thank you.....