Skip to main content
A.Caliskan
Associate III
January 6, 2022
Question

SPI UNDERRUN ERROR ??

  • January 6, 2022
  • 1 reply
  • 2415 views

Hello, ı m use stm32h750vb, I'm trying to use spi half duplex_tx in slave mode, When I transmit for the first time, it sends data, but then it does not. When I checked the registers, the udr flag seems to be set. Why is the Udr Flag 1?(I'm sending 16 pulses per second over the clock systict timer.

static void MX_SPI3_Init(void)
{
 
 /* USER CODE BEGIN SPI3_Init 0 */
 
 /* USER CODE END SPI3_Init 0 */
 
 LL_SPI_InitTypeDef SPI_InitStruct = {0};
 
 LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 LL_RCC_SetSPIClockSource(LL_RCC_SPI123_CLKSOURCE_PLL2P);
 
 /* Peripheral clock enable */
 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_SPI3);
 
 LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOC);
 /**SPI3 GPIO Configuration
 PC10 ------> SPI3_SCK
 PC11 ------> SPI3_MISO
 */
 GPIO_InitStruct.Pin = LL_GPIO_PIN_10|LL_GPIO_PIN_11;
 GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct.Alternate = LL_GPIO_AF_6;
 LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /* USER CODE BEGIN SPI3_Init 1 */
 
 /* USER CODE END SPI3_Init 1 */
 /* SPI3 parameter configuration*/
 SPI_InitStruct.TransferDirection = LL_SPI_HALF_DUPLEX_TX;
 SPI_InitStruct.Mode = LL_SPI_MODE_SLAVE;
 SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_16BIT;
 SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_HIGH;
 SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
 SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
 SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
 SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
 SPI_InitStruct.CRCPoly = 0x0;
 LL_SPI_Init(SPI3, &SPI_InitStruct);
 LL_SPI_SetStandard(SPI3, LL_SPI_PROTOCOL_MOTOROLA);
 LL_SPI_DisableNSSPulseMgt(SPI3);
 /* USER CODE BEGIN SPI3_Init 2 */
 
 /* USER CODE END SPI3_Init 2 */
 
}
 
/* USER CODE BEGIN 0 */
void SysTick_Handler(void)
{
 /* USER CODE BEGIN SysTick_IRQn 0 */
 
 /* USER CODE END SysTick_IRQn 0 */
 
 /* USER CODE BEGIN SysTick_IRQn 1 */
 
			if(count<=32)
			{
				LL_GPIO_TogglePin(GPIOB, LL_GPIO_PIN_10);
 
			}
			else if(count==100000)//100000
			{
 
				count=0;
				
			}
			else
			{
				LL_GPIO_ResetOutputPin(GPIOB, LL_GPIO_PIN_10);
 
			}
 
 
	
 
 
 /* USER CODE END SysTick_IRQn 1 */
}
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 
 
 LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
 
 NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
 
 
 NVIC_SetPriority(SysTick_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),15, 0));
 
 
 SystemClock_Config();
 
 
 PeriphCommonClock_Config();
 
 
 
 MX_GPIO_Init();
 MX_SPI3_Init();
 
 
 LL_SPI_Enable(SPI3);
 
 SysTick_Config(SystemCoreClock/100000);
 
 while (1)
 {
 
	 if(LL_SPI_IsActiveFlag_TXP(SPI3))
	 {
		 LL_SPI_TransmitData16(SPI3,0x2AAA);
 
	 }
 
 
 }
 
}

)

1 reply

TDK
January 6, 2022

An UDR flag means the master clocked the SCK line before you were able to send data to the SPI peripheral. Perhaps your master is using a high clock rate and asking for data quicker than you can keep up.

Once UDR is set, you need to clear it before continuing.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Visitor II
December 3, 2024

Does this mean the master would send data on MOSI, stop clk and disable CS/SS, wait a duration of time, enable CS/SS, and then read on MISO?