cancel
Showing results for 
Search instead for 
Did you mean: 

timer break interrupt

Srinath_03
Senior

hi im using stm32g474vet6 mcu , in that i am using tim1 for pwm generation , for protection im enabling all the 7 comparators and exrernal break input pin for pwm shutdown. comparator configuration and dac settings are correctly done.i dont know why the tim_bkin interuppt is not shutdown the pwm by mcu hardware itself.

 

by software im doing like this comparator output is detected and pwm is shutdown. but by hardware external input and internally comparator hardware is not working

 

if(HAL_COMP_GetOutputLevel(&hcomp1) == 1)

{

Rectifier.COMP_faults.COMP1_Idc=1;

}

if(HAL_COMP_GetOutputLevel(&hcomp2) == 1)

{

Rectifier.COMP_faults.COMP2_Vbc=1;

}

if(HAL_COMP_GetOutputLevel(&hcomp3) == 1)

{

Rectifier.COMP_faults.COMP3_Vab=1;

}

if(HAL_COMP_GetOutputLevel(&hcomp4) == 1)

{

Rectifier.COMP_faults.COMP4_Ia=1;

}

if(HAL_COMP_GetOutputLevel(&hcomp5) == 1)

{

Rectifier.COMP_faults.COMP5_Ib=1;

}

if(HAL_COMP_GetOutputLevel(&hcomp6) == 1)

{

Rectifier.COMP_faults.COMP6_VDC=1;

}

if(HAL_COMP_GetOutputLevel(&hcomp7) == 1)

{

Rectifier.COMP_faults.COMP7_Ic=1;

}

 

if((Rectifier.COMP_faults.COMP1_Idc) || (Rectifier.COMP_faults.COMP2_Vbc) || (Rectifier.COMP_faults.COMP3_Vab) || \

(Rectifier.COMP_faults.COMP4_Ia) || (Rectifier.COMP_faults.COMP5_Ib) || (Rectifier.COMP_faults.COMP6_VDC) || \

(Rectifier.COMP_faults.COMP7_Ic) )

{

__HAL_TIM_MOE_DISABLE(&htim1);

Rectifier.COMP_faults.COMP_FLAG = 1;

 

}

else

{

__HAL_TIM_CLEAR_FLAG(&htim1,TIM_FLAG_BREAK);

__HAL_TIM_MOE_ENABLE(&htim1);

Rectifier.COMP_faults.COMP_FLAG = 0;

 

}

 

1 REPLY 1
Karl Yamashita
Principal

Edit your post and use the </> to post code so it's formatted and readable 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source