How to use a same uart for two devices
Hello every one , i'm using a STM32L100RX, i am using PC11 and PC10 ports as USART3, so far everything it's okay, but i need to use the same usart (USART3) on the PB11 and PB10 pins...i need configure these pins in runtime because i have another device on it! something like multiplexor, so what i do?¿
this is my code:
GPIO_InitTypeDef def,def2;
HAL_GPIO_DeInit(GPIOB,GPIO_PIN_11); //Deinit port 11 and 10 of B PORT
HAL_GPIO_DeInit(GPIOB,GPIO_PIN_10);
def.Alternate = GPIO_AF7_USART3;
def.Pull = GPIO_NOPULL;
def.Mode = GPIO_MODE_AF_PP;
def.Pin = GPIO_PIN_11;
def.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOC,&def);
def2.Alternate = GPIO_AF7_USART3;
def2.Pull = GPIO_NOPULL;
def2.Mode = GPIO_MODE_AF_PP;
def2.Pin = GPIO_PIN_10;
def2.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOC,&def2); //Set now the usart 3 to the desired PORTbut it doesn't work...any idea?¿
Regards!